RX_FAULT_LOCATIONS

Field Name

Description

IDX

The unique ID assigned to the fault location.

OID

Object ID of the feature.

FCID

Feature class ID of the feature.

SUBID

The unique ID of each segment of a complex edge.

FACILITY_ID

The Facility ID of the incident feature as defined in the geodatabase.

X

The x-coordinate of the incident feature.

Y

The y-coordinate of the incident feature.

INCIDENT_ID

The ID associated with the incident. This field corresponds with the ID field in the RX_INCIDENTS table.

PROBABILITY

The percentage of probability that the fault location is accurate.

USER_CREATED

This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who created the record.

USER_UPDATED

This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.