TmScenarios Table

All of the following fields must exist in the TmScenarios table.

Field

Description

Scenario

A unique number identifying the scenario.

This field is a primary key.

Name

A description for the scenario.

Device Facility ID

The Facility ID of the outage device.

Device Type

The Type of the outage device.

DeviceFcid

Feature class ID for the incident device.

DeviceOid

Object ID for the incident device.

Customers Affected

The number of customers affected by the outage.

NumberCalls

The number of customers that called in the scenario.

NumberHazards

The number of hazards in the scenario.

Comments

Comments about the outage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.