Hide Operations

You have the option to hide operations in the Tasks category on the Switching Orders Editor. To do this, edit the Miner.Responder.Explorer.exe.config file on all client machines.

To set this option, follow the steps outlined below.

  1. On the client machine, browse to and open Miner.Responder.Explorer.exe.config. By default, this file is installed here: C:\Program Files (x86)\Miner and Miner\Responder\Client.
  2. Locate the following XML.
         <add key="Switching.HiddenTasks" value="None"/>
  3. In the value field, type a comma-separated list of tasks to hide. Valid values are listed in the Value field:

    Operation Name

    Value

    Close Device

    CloseDevicePhases

    Open Device

    OpenDevicePhases

    Place Cut

    PlaceCut

    Repair Cut

    RepairCut

    Device Information

    DeviceInformationTask

    Information

    InformationTask

    Place 'Do Not Close' Tag

    PlaceDoNotCloseTag

    Place 'Do Not Isolate' Tag

    PlaceDoNotIsolateTag

    Place 'Do Not Open' Tag

    PlaceDoNotOpenTag

    Place 'Do Not Operate' Tag

    PlaceDoNotOperateTag

    Place 'Future Work Required' Tag

    PlaceFutureWorkRequiredTag

    Place Ground

    PlaceGround

    Place 'Information' Tag

    PlaceInformationTag

    Remove Ground

    RemoveGround

    Remove Tag

    RemoveTag

  4. Save and close Miner.Responder.Explorer.exe.config.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.