RX_INCIDENT_FEATURES

Much of the data in this table may be viewed on the Responder Explorer Incidents tab by right-clicking a location feature and selecting Edit.

Field Name

Description

OID

Object ID of the feature associated with the incident.

FCID

Feature class ID of the feature associated with the incident.

SUBID

The unique ID of each segment of a complex edge.

X

The x-coordinate of the incident feature.

Y

The y-coordinate of the incident feature.

INCIDENT_ID

The ID associated with the incident. This field acts as a foreign key to the RX_INCIDENTS table.

TIME_REPORTED

Time that the feature was reported out.

CONFIRMED

Indicates whether the feature has been confirmed out. This field uses the CONFIRMED domain.

FACILITY_ID

The Facility ID of the incident feature as defined in the geodatabase.

USER_CREATED

The name of the user who created the record. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the record. This field is populated automatically by Responder.

REMARKS

Notes from the operator or dispatcher.

REGION

The region in which the device resides. This field uses the REGION domain.

CANCEL_REASON

Reason the feature was cancelled.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.