Data Preparation

Perform the following tasks to prepare your data to be used with Responder. Responder requires that the data have the following configurations completed before starting the configuration steps below: Basic ArcFM and Feeder Manager.

Archiving: If you choose to use GlobalIDs, they must be added to the geodatabase BEFORE archiving is enabled.

IMPORTANT: Responder requires the descriptions in the FdrMgrVoltageCode domain be created so that increasing voltages map to increasing description values in the Operating Voltage domain. See the Voltage Code Domains page in the Feeder Manager section for more information.
  • Add Model Names

  • Assign Model Names

  • Display De-Energized Feeders (optional)

  • Display Jumpers (optional)

  • Load point trace weight update

  • Populate Customer Data

  • Database Schema (optional)

  • Set Up Responder Map Layers

  • Regions

  • Create Network Level Field (optional)

  • Address Field (optional)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.