Data Services Console

Use the console to manage your existing instances of Data Services. By default, the Configuration screen is displayed. Click the Console link to manage your Data Services. .

If you are running multiple instances of Data Services, there will be multiple console windows (one for each instance). To use a command, enter it in the Input field and click Send. The results of the command are displayed in the windows for each Data Services instance running. The various commands you can use in this window are listed here

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.