9.3 SP1 Upgrade Scripts - Oracle

The following implementation scripts must be run on your Responder Oracle database to add the correct tables, views, and indices to upgrade Responder to version 9.3 SP1. When upgrading Responder execute ONLY the Upgrade script(s) that fall between your previous release and the new release to which you are upgrading. Do NOT execute any Implementation Scripts.

With the release of 9.3 SP1, the Implementation scripts have been modified to change a few fields. These modifications are not in the upgrade scripts and should be made manually. Those marked with an asterisk (*) are required. All others listed below are optional. These changes must be made consistently across all Responder tables in all databases.

  • Change the length of the Region, RegionID, and Owner fields to 38.

  • Change the length of the Mobile_Phone and Home_Phone fields to 15 (RX_CREW_MEMBERS, RX_CREW_MEMBER_ARCHIVE, RX_CREW_MEMBERS_HISTORY tables).

  • International Utilities Only: Change fields with a type of varchar2 to nvarchar2.

Responder requires two schemas: Responder and Archive. Some scripts are run on the Responder schema and some on the Archive schema. In the list below, the schema on which the script should be executed is in parentheses.

  • 930sp1_01_RxTables_oracle.sql (Responder)

  • 930sp1_02_ArchiveTables_oracle.sql (Archive)

  1. Log in to the Responder schema as RESPONDER (i.e., schema owner). Use an application such as SQL Plus.
  2. Execute the 930sp1_01_RxTables_oracle.sql script by entering "@" followed by a path to the script (an example follows) and pressing Enter. This script creates the database tables required by Responder.
    @ D:\Program Files\Miner and Miner\Responder\Developer Resources\
    9.3.0 - 9.3.0 SP1 Upgrade Scripts\Oracle\930sp1_01_RxTables_oracle.sql
  3. Log in to the Archive schema as ARCHIVE (i.e., schema owner).
  4. Execute the 930sp1_02_ArchiveTables_oracle.sql script in the same manner as the first script. Enter "@" followed by a path to the script and press Enter. This script creates the database tables required by Responder Archive Explorer.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.