Switch Order Tab Name

The setting here allows you to control which value for a Switch Order appears in larger font on the Switch Order Editor window > Switch Order tab. You can elect to display either the Name of the Switch Order or the ID as the emphasized text on the Switch Order tab. The other value then appears below the emphasized text in a smaller font on the tab.

Name Emphasized ID Emphasized

  1. Open Miner.Responder.Explorer.exe.config. By default, this file is installed here: C:\Program Files (x86)\Miner and Miner\Responder\Client.
  2. Look for the following XML:
    <add key="Switching.TabHeaderPrimaryDisplay" value="Name" /> 
  3. To display the Switch Order ID as the emphasized text, set the value to ID. By default, it is set to Name.
  4. Save and close Miner.Responder.Explorer.exe.config.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.