RX_SW_OR_REQUESTS_ARCHIVE

Field Name

Description

SW_OR_REQUESTS_ID

The ID associated with the switching order request.

INCIDENT_ID

The ID associated with the incident resulting from the call. This field corresponds with the ID field in the RX_INCIDENTS table.

TOTAL_CUSTOMERS_COUNT

The total number of customers affected by the switching order request.

CRITICAL_CUSTOMERS_COUNT

The number of critical customers affected by the switching order request.

PRIORITY_CUSTOMERS_COUNT

The number of priority customers affected by the switching order request.

NAME

The name associated with the switching order request.

PHONE_NUMBER

The phone number associated with the switching order request.

FEEDER_ID

The ID of the feeder.

REGION

The region in which the switching order feature is located. This field uses the REGION domain.

SHORT_DESCRIPTION

The short description provided with the switching order request.

REQUEST_REFERENCE

The reference number assigned to the request.

PLANNED_BEGIN_TIME

The planned time for the work in the request to begin.

PLANNED_END_TIME

The planned time for the work in the request to be completed.

REASON

The reason provided for the switching order request.

STATUS

The status of the switching order request.

USER_CREATED

The name of the user who created the record. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the record. This field is populated automatically by Responder.

CHANGE_DATE

The time and date an operation was performed on the record.

OPERATION

The operation (e.g., insert, delete, update) performed on the record.

USER_UPDATED_ARCH

This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record.

SWITCHING_ORDER_ID

The unique ID that identifies the switching order to which the request has been assigned.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.