RX_TAGS_AND_GROUNDS_ARCHIVE
|
Field Name |
Description |
|---|---|
|
TAG_AND_GROUND_ID |
A unique identifier for a tag or ground. This field corresponds to the ID field in the RX_TAGS_AND_GROUNDS table. |
|
TAG_ID_1 |
ID of the tag. |
|
TAG_ID_2 |
ID of the tag. |
|
TAG_ID_3 |
ID of the tag. |
|
FCID |
Feature class ID of the feature associated with the tag. |
|
OID |
Object ID of the feature associated with the tag. |
|
SUBID |
The unique ID of each segment of a complex edge. |
|
X |
The x-coordinate of the incident device. |
|
Y |
The y-coordinate of the incident device. |
|
TAG_TYPE |
Indicates the type of tag (e.g., Information, Do Not Operate, Do Not Close). |
|
PHASES |
Indicates which phases are affected. |
|
GROUND |
Indicates whether the step is a ground (yes/no). |
|
FACILITY_ID |
The Facility ID of the incident device as defined in the geodatabase. |
|
REGION |
The region in which the tag or ground is located. This field uses the REGION domain. |
|
OWNER |
The tag owner (who placed the tag). |
|
TIME_PLACED |
Time that the tag was placed. |
|
TIME_REMOVED |
Time that the tag was removed. |
|
REMARKS |
Remarks associated with the tag. |
|
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
|
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
|
CHANGE_DATE |
The time and date an operation was performed on the record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the record. |
|
USER_UPDATED_ARCH |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record. |
|
ORIGINATION |
Indicates where the tag was originated (i.e., manual or switching order). Any tags originated within a switching order may not be deleted in the Tags window. |
|
SUMMARY |
The summary text provided on the tag. |
|
OWNER_NAME |
The name of the tag's owner. |
|
TAG_GUID |
The GUID assigned to the tag. |
|
FEATURE_CLASS_NAME |
The name of the Feature Class on which the incident occurred, as it was configured/named when the Incident was archived. |