Telemetry Service Descriptions

NOTE: In the table below, the values of the Category column refer to:
  • Database: Metric capturing time to perform an insert, update, delete, or read on the database

  • Detail: Metric capturing one specific element of a process in the code

  • Service: Metric capturing service performance on a server machine

  • User: Metric based on performance of a specific Responder function that an end user would experience

Telemetry Item

Category

Description

ArchiveExplorer.GenerateReport

User

Occurs when the user selects Archive Report and clicks Generate Report in Archive Explorer. The telemetry value represents the time to generate the specified report. Gives information about report type - report name. Next to this telemetry value is always additional information with report request details - request and data filter.

ArchiveExplorer.Refresh

User

Occurs when the user clicks Refresh in Archive Explorer. The telemetry value represents the length of time to perform a full refresh per grid. Gives information about the Refresh applying to Incidents Archive or Tag Archive data and information about number of refreshed rows.

ArchiveIncidents.GetIncidentData

Detail

Occurs as part of ArchiveIncidents. The telemetry value represents the length of time to perform reaching history data from database. Gives more details about the Incident for archiving and applied filters.

ArchiveIncidents.InternalArchive

Detail

Occurs as part of ArchiveIncidents. The telemetry value represents the length of time to perform archiving data. Gives more details about number of archived Incidents.

ArchiveServices.ApplyPostSubmitRules

Detail

Occurs as part of ArchiveServices.Submit. The telemetry value represents the length of time to perform PostSubmit rules.

ArchiveServices.ApplyPreSubmitRules

Detail

Occurs as part of ArchiveServices.Submit. The telemetry value represents the length of time to perform PreSubmit rules.

ArchiveServices.ArchiveIncidents

Service

Occurs when an Incident is closed. If Archive Service is started, Data Service sends a request to Archive Service. The telemetry value represents the length of time to perform archiving incidents.

ArchiveServices.ArchiveTags

Service

Occurs when a Tag is removed. If Archive Service is started, Data Service sends a request to Archive Service. The telemetry value represents the length of time to perform archiving tags.

ArchiveServices.Submit

Service

Occurs after changing an Incident or a Tag in Archive Explorer. The telemetry value represents the length of time to perform applying submit rules to changed data before writing to database.

BuildArchive.Incidents

Detail

Occurs when the user click Build Archive in Archive Explorer. The telemetry value represents the time it takes to build the Incidents archive from history tables.

BuildArchive.Tags

Detail

Occurs when the user click Build Archive in Archive Explorer. The telemetry value represents the time it takes to build the Tags archive from history tables.

CallManagement.EnsureReferentialIntegrity

Detail

Captures duration of loading missing tables (RX_INCIDENTS and RX_INCIDENT_DEVICES). It is called when call is associated to incident (in prediction and some submit rules).

CancelIncident.Complete

User

Occurs when cancelling an incident in Responder Explorer. The telemetry value represents the time it takes from when user clicks on the OK\Cancel button to the moment when operation is finished and UI is available.

CancelIncident.Open

User

Occurs when cancelling an incident Responder Explorer. The telemetry value represent the time it takes to open the cancel incident dialog.

ChangeQuery

User

Occurs when the user changes a query in Archive Explorer (example, switch to "Incidents by Region"). The telemetry value represents the length of time to perform refreshing grid according new query. Gives information about chosen query and query criteria.

CleanupIncidentDeviceErrors.EnsureReferentialIntegrity

Detail

Captures duration for this method. It loads missing tables into dataset. It is called from CleanupIncidentDeviceErrors submit rule.

CleanupIncidentDeviceErrors.QueryForExistingIncidentDevice

Detail

Captures duration for this method. It is called from CleanupIncidentDeviceErrors submit rule.

CloseIncident.Complete

User

Occurs when closing an incident in Responder Explorer. The telemetry value represents the time from the user clicking OK/Cancel to when the incident is closed and UI is available again.

CompleteIncident.Complete

User

Occurs when the Complete Incident operation is run. The telemetry value represents the time it takes from when user runs the Complete incident command to the moment when incident is completed in grid and UI is available again.

Database.ExecuteNonQuery

Database

Records the SQL (insert, update, delete) text and how long each query takes to execute.

Database.ExecuteScalar

Database

Records the SQL query text and how long each query takes to execute.

Database.ExecuteReader

Database

Records the SQL query text and how long each query takes to execute.

Database.ExecuteDataTable

Database

Records the SQL query text and how long each query takes to execute.

DataManager.RefreshAll

Detail

Captures the duration of a full (manual) refresh. This is different from ResponderExplorer.ManualRefresh as this can get called even when the user doesn't ask for it - as when an optimistic concurrency issue happens during a submit and the client needs a refresh of data.

DataManager.Submit

Detail

Occurs when a DataSet is "submitted" to DataServices for processing.

DataManager.PartialRefresh

Detail

Captures the duration of a partial refresh (sometimes referred to as "soft refresh"). Is the outer-most one and most closely matches the "soft refresh" user experience metric. It is called in 3 places, including soft refresh, full refresh, and in some conditions during a submit.

DataManager.Reinitialize

Detail

Captures the duration of a "reinitialize" (a heavier-weight refresh than "refresh all")

DataServices.ApplyPostSubmitRules

Detail

Occurs as part of DataService. The telemetry value represents the time it takes to process all post-submit rules.

DataServices.ApplyPreSubmitRules

Detail

Occurs as part of DataService. The telemetry value represents the time it takes to process all pre-submit rules.

DataServices.ExecuteRequest

Service

Records the length of time each DataRequest takes to execute. The telemetry value indicates the length of time (in seconds) and the message (description) indicates the name of the DataRequest. DataRequests that take less than 1 second may not be recorded.

DataServices.SubmitForPrediction

Detail

Captures how long it takes to process the submitted DataSet and send the resulting information to PredictionServices.

DataServices.Submit

Service

The common method called by both IDataServices.Submit and SubmitDataRequest.

DataServicesProxy.ExecuteRequest

Detail

Captures how long a client waits (client-side) for DataServices.ExecuteRequest to be called. The difference between this telemetry and DataServices.ExecuteRequest includes network time.

DataWriter.Write.Added

Detail

Captures the duration of adding rows to Data Services and how many rows were created. This does not include post-processing time.

DataWriter.Write.Deleted

Detail

Captures the duration of removing rows from Data Services and how many rows were removed. This does not include post-processing time.

DataWriter.Write.Modified

Detail

Captures the duration of editing rows in Data Services and how many rows were changed. This does not include post-processing time.

ExplorerData.ApplyPubSubChanges

Detail

Captures the duration of applying pub/sub changes.

GenerateReport.ExportToXML

Detail

Occurs on Generate Report in Archive Explorer. Represents time for serializing dataset (QueriesHelper.GenerateDataSet) to XML file.

GenerateReport.Transform

Detail

Occurs on Generate Report in Archive Explorer. Represents time for applying XSLT transformation to XML file (GenerateReport.ExportToXML exported file).

IDM.FindFeedPath

Detail

IDM find feed path.

IDM.FindModifiedElements

Detail

IDM find modified elements, this will get the energized and deenergized elements in IDM.

IDM.GetDownstreamConfirmedSPIs

Detail

Occurs as part of DataService. Occurs if current processing device is loadpoint. Includes trace for finding all devices which are not services points with confirmed incidents, and than by getting difference with all devices (deenegized\energized) gets downstream confirmed SPIs.

IDM.HandleDifferentlyEnergizedElements

Detail

Occurs as part of DataService. Occurs when currently processing device causes that some downstream devices are differently energized.

IDM.ProcessCanceledOrDeletedDevice

Detail

Occurs as part of DataService. Occurs when currently processing device is deleted or cancelled.

IDM.ProcessDevice

Detail

Occurs as part of DataService. Occurs when a device is added, deleted or modified. The telemetry value represents the time to do processing device in IDM.

IDM.RollUp

Detail

Occurs as part of DataService. Occurs when incident of currently processing device is rolled up.

IDM.SelectResponsibleStopperDeviceRow

Detail

Occurs as part of DataService. Occurs when currently processing device has newly energized or deenergized phases and no new loadpoints.

IDM.SharedIncidentLoadpoints

Detail

Captures duration of this IDM processing part. Occurs when a loadpoint already exists for other incidents.

IDM.UpdateIncidentCustcounts

Detail

Occurs as part of DataService. Occurs when customer count on incident of processing device should be updated.

IDMLoadpointsHelper.ProcessDeEnergizedLPs

Detail

Captures duration of this IDM processing part.

IDMLoadpointsHelper.ProcessLoadpointsAndTransformers

Detail

Captures duration of this IDM processing part.

IncidentDevice.IsDeviceUnderInfluenceOfDifferentIncident

Detail

Captures duration of this IDM processing part.

Prediction.AnalyzeCalls

Detail

"Analyze calls" command in Responder Explorer results in creation of AnalyzeCallsRequest and asynchronous call of AnalyzeCalls method on Prediction Service. Telemetry result contains elapsed time and number of calls processed during that period.

Prediction.CalculateImmediateChildOutageRatio

Detail

Captures duration for this method.

Prediction.CreateOrModifyExistingIncident

Detail

Occurs in InternalPrediction.AnalyzeCall. This measurement gives better understanding why some AnalyzeCall takes more or less time.

Prediction.Predict

Detail

Occurs in couple events - AnalyzeCalls and PredictOnDataset (these two events are measuring separately as well). Telemetry log contains resulted device - "predicted device" information, if predicted device exists, otherwise just time value.

Prediction.PredictOnDataSet

Detail

Predict on dataset is calling asynchronously and if input dataset is not "marked" as predicted than it goes in this procedure.

Prediction.SubmitAsProbableStateCandidate

Detail

Occurs as part of PredictOnDataset event and Probable state polling extension (periodical checking). If probableStateCandidateElevationTime (Threshold Info attribute) expires then all devices which are candidates for changing state to Probable will be processed in this method.

PredictionServices.AnalyzeCalls

Detail

"Analyze calls" command in Responder Explorer results in creation of AnalyzeCallsRequest and asynchronous call of AnalyzeCalls method on Prediction Service. Telemetry represents full time for precessing all submitted calls and gives number of calls processed in this period.

QueriesHelper.GenerateDataSet

Detail

Occurs on Generate Report in Archive Explorer. Telemetry log represents time for generating dataset for specified report and also show additional information about report query.

QueryService.ExecuteRequest

Service

The length of time it takes to execute a DataRequest in Query Services.

QueryServicesLocalProxy.ExecuteRequest

Detail

This is a QueryServices local proxy (for use inside QS) and indicates how long it takes to call ExecuteRequest. This is used for DataRequests that call other DataRequests inside QueryServices.

RegionModeAssignment.GetRegionModeAssignmentList

Detail

Occurs when Region Mode Assignments is initializing first time or after RegionModeAssignment multicast event handler clear cache. Telemetry value represents the length of time for initializing Region Mode Assignments.

ResponderExplorer.ManualRefresh

User

Occurs when the user clicks Refresh in Responder Explorer. The telemetry value represents the length of time to perform a full refresh.

ResponderExplorer.StartupTime

User

Occurs during the startup of Responder Explorer. The telemetry value represents the time it takes to start Responder Explorer.

SubmitDataWriter.Write

Detail

Records the length of time it takes to record (local) changes in the DataSet to the database. This includes some number of insert, update, and delete statements.

SubmitRule.ApplyRule

Detail

Records the duration of executing a particular submit rule. This event is only recorded for operations that take longer than 1 second.

Tracing.FindFeedPath

Detail

General Find Feed Path.

Tracing.DownStreamTrace

Detail

General Find DownStream Trace.

Tracing.FindChildDevices

Detail

Find Child devices below a device.

UpgradeArchive.Incidents

User

Occurs when the user clicks Upgrade Archive in Archive Explorer. The telemetry value represents the time it takes to upgrade archive according history data.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.