Require Removal of All Tags
By default, a user can restore or cancel a device in a switching order even if all tags have not been removed (e.g., tag for future repairs). You can modify this behavior and require all tags be removed before the device can be restored or cancelled and the switching order closed. To do this, follow the steps below.
- On the Responder server, browse to ExplorerRulesConfig.xml. By default this file is installed here: C:\Program Files (x86)\Miner and Miner\Responder\Server.
- Open ExplorerRulesConfig.xml. ExplorerRulesConfig.xml can be edited using an XML application (such as XML Spy) or by opening it in a simple text editing program (such as Notepad).
-
Locate the following XML:
<RulePackage Key="TagDeleteInitialization" Caption=""> <b:RuleClasses Key=""> <!--<b:RuleClass Key="InitializeTagForDelete" Type="Miner.Responder.Explorer.InitializationRules.InitializeTagForDelete,Miner.Responder.Explorer" />--> <b:RuleClass Key="DataRowRule" Type="Miner.Data.Access.DataRowRule,Miner.Data.Access"/> </b:RuleClasses> </RulePackage>
-
Remove the comment marks from the InitializeTagForDelete
key. So it looks like this:
<RulePackage Key="TagDeleteInitialization" Caption=""> <b:RuleClasses Key=""> <b:RuleClass Key="InitializeTagForDelete" Type="Miner.Responder.Explorer.InitializationRules.InitializeTagForDelete,Miner.Responder.Explorer" /> <b:RuleClass Key="DataRowRule" Type="Miner.Data.Access.DataRowRule,Miner.Data.Access"/> </b:RuleClasses> </RulePackage>
- Save and close ExplorerRulesConfig.xml.