Open Web Dashboard

The Open Web Dashboard button allows the user to easily open and view the Responder Dashboard. This button must be configured to point to the correct URL.

  1. Open Miner.Responder.Explorer.exe.config. This file is installed in: Program Files\Miner and Miner\Responder\Client\.
  2. Look for the following line of XML:
    <add key="DashboardURL" value="http://Waldo/Responder/Dashboard/Default.aspx"/>
  3. Modify the path to the web server. In the example above, Waldo is the name of the Responder web server.
  4. Save and close Miner.Responder.Explorer.exe.config.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.