RX_REGION_CUSTOMERS

This table is used to archive the number of customers within a specific region at a given point in time.

Field Name

Description

COUNT_DATE

Date the count was taken of all customers in the region.

REGION_ID

The ID of the region.

CUSTOMER_COUNT

Indicates the number of customers affected by the incident.

CRITICAL_CUSTOMER_COUNT

Indicates the number of critical customers affected by the incident.

PRIORITY_CUSTOMER_COUNT

Indicates the number of priority customers affected by the incident.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.