RX_TRUCKS

Populate this table with your truck information.

Field Name

Description

REGION

The region in which the truck is located. This field uses the REGION domain.

TRUCK_TYPE

The type of truck.

RADIO1

The radio frequency at which the crew can be reached.

RADIO2

An alternative radio frequency at which the crew can be reached.

COMPANY

The company to which the truck belongs. This field uses the COMPANY domain.

STATUS

The status of the truck. This field uses the STATUS domain.

CREW_ID

Indicates the crew to which the truck is assigned. This field acts as a foreign key to the RX_CREWS table.

USER_CREATED

The name of the user who created the record. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the record. This field is populated automatically by Responder.

TRUCK_NUMBER

This optional field holds company ID values (e.g., license plate numbers, inventory numbers). This string field holds up to 15 characters.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.