48049-137-05EN

Adjustable Rating Plug Replacement

NOTE: To select correct replacement rating plug, see the product catalog.
NOTE: Adjustable rating plug must be removed when doing hi-pot testing. Adjustable rating plug must be installed for voltage measurement. If adjustable rating plug is removed, the circuit breaker will default to a long-time pickup rating of 0.4 x sensor size (In) and a long-time delay of whatever setting was selected before the rating plug was removed.
DANGER
hazard of electric shock, explosion, or arc flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462, NOM 029-STPS or local equivalent.
  • This equipment must be installed and serviced only by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment. Follow instructions shipped with circuit breaker to disconnect and reconnect circuit breaker.
  • Replace all devices, doors and covers before returning equipment to service.
Failure to follow these instructions will result in death or serious injury.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.