48049-137-05EN

Remove Rating Plug

  1. Disconnect circuit breaker as directed in the circuit breaker instruction bulletin shipped with the circuit breaker.

  2. Open switch cover (A).

  3. Record switch settings in Appendix E (switch settings and those set with graphic screen, if applicable).

  4. Unscrew plug mounting screw (B).

  5. Remove adjustable rating plug (C).

Remove Adjustable Rating Plug

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.