48049-137-05EN

Ground-Fault Protection for Equipment

Ground-Fault Protection Switches

Equipment ground-fault protection protects conductors against overheating and faults from ground-fault currents (≤ 1200 A).

  • Equipment ground-fault protection is standard on 6.0P trip units.

  • Ground-fault pickup (Ig) (A) sets ground current level where circuit breaker will trip after the preset time delay.

  • Ground-fault delay (tg) (B) sets the length of time that the circuit breaker will carry a ground-fault current above the ground-fault pickup current level before tripping.

  • Equipment ground-fault protection can be zone-selective interlocked (ZSI) with upstream or downstream circuit breakers. Setting the ground-fault delay (tg) to the 0 setting turns off zone-selective interlocking.

  • Neutral protection and equipment ground-fault protection are independent and can operate concurrently.

NOTE: Use I2t off with ZSI for proper coordination. Using I2t on with ZSI is not recommended as the delay in the upstream device receiving a restraint signal could result in the trip unit tripping in a time shorter than the published trip curve.

MicroLogic Trip Unit Ground-Fault Pickup Values

Ig (= In x....) A B C D E F G H J
In ≤ 400 A 0.3 0.3 0.4 0.5 0.6 0.7 0.8 0.9 1
400 A < In ≤ 1200 A 0.2 0.3 0.4 0.5 0.6 0.7 0.8 0.9 1
In > 1200 A 500 A 640 A 720 A 800 A 880 A 960 A 1040 A 1120 A 1200 A

In = sensor rating.
Ig = ground-fault pickup.

MicroLogic Trip Unit Ground-Fault Delay Values

Setting Ground-Fault Delay
I2t off (ms at In) (seconds) 0 0.1 0.2 0.3 0.4
I2t on (ms at In) (seconds) 0.1 0.2 0.3 0.4
tsd (min. trip) (milliseconds) 20 80 140 230 350
tsd (max. trip) (milliseconds) 80 140 200 320 500
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.