48049-137-05EN

Contact Wear Indicator

The trip unit keeps track of the circuit breaker contact wear when a MasterPact circuit breaker type is selected. The amount of wear on the circuit breaker contacts can be transferred when a trip unit is replaced. (External trip unit power supply is required.)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.