48049-137-05EN

Minimum (Under) and Maximum (Over) Demand Current and Voltage Protection

Minimum/Maximum Protection Curves

Maximum Protection

Minimum Protection

Provides pickup and dropout values for alarm, contacts or tripping for current and voltage values. (There is no minimum for current.)

  • Pickup value (A) is set to activate an alarm or trip.

  • Pickup time delay (B) is set to start timing once the pickup value has been passed.

  • Dropout value (C) is set to deactivate the alarm and/or contact.

  • Dropout time delay (D) is set to start timing once the dropout value has been passed.

  • Minimum (under) voltage protection (Vmin) is activated when any line-line voltage is below the minimum voltage setting.

  • Maximum (over) voltage protection (Vmax) is activated when any line-line voltage is above the maximum voltage setting.

  • Vmin has a dropout value ≥ pickup value.

  • Vmax has a dropout value ≤ pickup value.

  • If current or voltage protection trips the circuit breaker, the circuit breaker cannot be reset until the current or voltage problem which caused the trip is corrected.

  • Ground-fault alarm on the 5.0P and 6.0P trip unit is based on true rms value of the ground current.

  • Do not set undervoltage protection below 80%.*

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.