48049-137-05EN

Protection Setup

Use the protection menus to check protection setup for amperage protection, voltage protection, other protection, current load shedding and power load shedding.

Refer to Appendix B for default settings and setting ranges.

Protection Menu

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.