48049-137-05EN

Introduction

MicroLogictrip units provide adjustable tripping functions on electronic trip circuit breakers. The product name (A) specifies the level of protection provided by the trip unit.

MicroLogic trip units are field replaceable to allow for upgrading of the trip unit in the field. For complete information on available circuit breaker models, frame sizes, interrupting ratings, sensor plugs, rating plugs and trip units, see the product catalog.

MicroLogic Trip Unit

     
  A Product Name
  B Trip Indicators
  C Battery Housing
  D Adjustable Switches
  E Switch Cover
  F Sealing Tab
  G Adjustable Rating Plug
  H Reset Button for Battery Status Check and Trip Indicators
  I External Terminal Block Connection
     
     
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.