48049-137-05EN

Power Load Shedding

Power load shedding can be configured for alarm only. It cannot be used to trip the circuit breaker.

NOTE: Press Protection button to view Protection Menu.

Check Power Load Shedding

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.