48049-137-05EN

Power and Control Settings

Using the graphic display screen and keypad on the trip unit, trip unit options can be set or system measurements checked. See Graphic Display Navigation for more information. System measurements can also be checked using the System Manager Software (SMS), Version 3.2 or later, or other network system management software.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.