48049-137-05EN

Load Shedding

Load shedding does not trip the circuit breaker, but may be used to activate an alarm linked to an M2C or M6C contact (controlling non-priority network loads).

  • Load shedding is defined by a threshold and time delay:

    A—Activation threshold

    B—Activation time delay

    C—Dropout threshold

    D—Dropout time delay

  • Power load shedding depends on the flow direction set during trip unit setup.

  • Current load shedding is connected to the I2t or Idmtl long-time delay values.

  • Current load shedding cannot be activated if “Long-time OFF” rating plug is installed.

Load Shedding

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.