48049-137-05EN

MicroLogic 6.0P Trip Unit

6.0P Trip Unit

     
  A Graphic display screen
  B

Protection menu button (Button includes an LED indicating the active menu)

  C

Maintenance menu button (Button includes an LED indicating the active menu)

  D

Metering menu button

  E

Down button

  F

Up button

  G

Enter button

  H

Long-time pickup (Ir) switch

  I

Long-time delay (tr) switch

  J

Short-time pickup (Isd) switch

  K

Short-time delay (tsd) switch

  L

Instantaneous pickup (Ii) switch

  M

Ground-fault protection pickup (Ig) switch

  N

Ground-fault protection delay (tg) switch

  O

Test plug receptacle

  P

Ground-fault push-to-trip button

  Q

Long-time pickup overload indicator light

  R

Reset button for battery status check and trip indicator LED

  S

Self-protection and advanced-protection indicator light

  T

Ground-fault trip indicator light

  U

Short-time or instantaneous trip indicator light

  V

Long-time trip indicator light

     
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.