48049-137-05EN

M2C and M6C Programmable Contact Kits

One or more alarms can be activated using an optional M2C or M6C programmable contact kit. The M2C contact kit provides two form A contacts with common neutral. The M6C contact kit provides six form C contacts. Each contact can be programmed through the trip unit for one alarm condition.

A 24 Vdc, 5 W auxiliary power supply is required for operation of trip unit/M2C or M6C contact kit combination.

NOTE: Trip unit and communication modules (BCM and CCM) must use separate power supplies. The M2C and M6C contact kits can share the trip unit auxiliary power supply.
Characteristics for M2C/M6C Programmable Contacts V A
Minimum Load 24 Vdc 100 mA
Breaking Capacity at a Power Factor (p.f.) of 0.7 240 Vac 5 A
380 Vac 3 A
24 Vdc 1.8 A
48 Vdc 1.5 A
125 Vdc 0.4 A
250 Vdc 0.15 A

M2C/M6C Wiring Diagrams

M2C: 24 Vdc power
supplied by trip unit
M6C: external 24 Vdc
power supply required
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.