48049-137-05EN

Metering Setup

Use “Metering setup” menu to set parameters for metering system current and power.

Metering Setup

  1. Select system type.

    Three measurement options are available:

    Network Type Neutral Phase Current
    3-phase, 3-wire, 3 CT (Uses 2 wattmeters) No Ia, Ib and Ic measured
    3-phase, 4-wire, 4 CT* (Uses 3 wattmeters) Yes Ia, Ib, Ic and In measured
    3-phase, 4-wire, 3 CT (Uses 3 wattmeters) No Ia, Ib and Ic measured
    NOTE: In the case of a four-pole circuit breaker, the ability to set the neutral is limited by the setting of the neutral type switch on the circuit breaker.

    In measurement is not available for “3phase, 4-wire, 3 CT” network types and Van, Vbn and Vcn simple voltage measurements are not available for “3phase, 3-wire, 3 CT” network types.

    If these measurements are desired, and if the connected system is a wye (4-wire) system, select “3-phase, 4-wire, 4 CT’ and connect to neutral (Vn) voltage terminal on the neutral CT.

    Set System Type

2.

Set current calculation method and interval.

The calculation method can be block interval or thermal calculation.

The window type is factory set as a sliding window.

The time interval can be set from five to 60 minutes in one minute increments.

Set Current Demand

3.

Set power calculation method and interval.

The calculation method can be block interval, thermal calculation or sync. to comms.

NOTE: The sync to comms method is available only with the communication option. This function determines demand power based on a signal from the communication module.

The default window type is sliding.

The time interval can be set from five to 60 minutes in one minute increments.

Set Power Demand

4.

Select sign convention.

Choose the signing convention to be used for reactive power (VARS) and reactive energy (VARhrs) and power factor measurements:

IEEE

IEC

IEEE alt

Set Sign Convention

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.