48049-137-05EN

Current Load Shedding

Current load shedding can be configured for alarm only. It cannot be used to trip the circuit breaker.

Check Current Load Shedding

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.