48049-137-05EN

MicroLogic 6.0P Trip Unit

  1. Set switches:

    A—Long-time pickup (Ir)

    B—Long-time delay (tr)

    C—Short-time pickup (Isd)

    D—Short-time delay (tsd)

    E—Instantaneous pickup (Ii)

    F—Ground-fault pickup (Ig)

    G—Ground-fault delay (tg)

  2. Fine-tune adjust using keypad and graphic display screen or the network system management software.

    Set Pickup Levels

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.