48049-137-05EN

Alarm History

The trip unit records measurement at each of the last ten alarms activated. For each alarm the following are stored:

  • Indication and value of the alarm setting

  • Date

  • Time (hour, minute and second)

Check Alarm History

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.