48049-137-05EN

MicroLogic 5.0P Trip Unit

5.0P Trip Unit

     
  A Graphic display screen
  B

Protection menu button (Button includes an LED indicating the active menu)

  C

Maintenance menu button (Button includes an LED indicating the active menu)

  D

Metering menu button

  E

Down button

  F

Up button

  G

Enter button

  H

Long-time pickup (Ir) switch

  I

Long-time delay (tr) switch

  J

Short-time pickup (Isd) switch

  K

Short-time delay (tsd) switch

  L

Instantaneous pickup (Ii) switch

  M

Test plug receptacle

  N

Long-time pickup overload indicator light

  O

Reset button for battery status check and trip indicator LED

  P

Self-protection and advanced-protection indicator light

  Q

Short-time or instantaneous trip indicator light

  R

Long-time trip indicator light

     

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.