48049-137-05EN

Trip Unit Resetting

Reset Trip Unit

When the circuit breaker trips, the fault indicator will remain lit until the trip unit is reset.

Do not return circuit breaker to service until cause of trip is determined. For more information, refer to the circuit breaker installation instructions shipped with the circuit breaker.

Press the reset/test button (A) to reset the trip unit after trip.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.