48049-137-05EN

Required Tools

  • Torque-controlled screwdriver, set at 7 inlbs (0.8 N•m) ± 10% (Lindstrom torque driver MAL500-2 or equivalent)

  • MicroLogic Full-Function Test Kit (part number S33595)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.