48049-137-05EN

Trip Unit Parameters Adjustment

NOTE: The protection menu settings cannot be adjusted unless the switch cover is open. When settings have been adjusted, press one of the menus buttons to save the new values.
  1. Open switch cover (A).

  2. Press maintenance button (B) to bring up maintenance menu (C).

Maintenance Menu

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.