48049-137-05EN

Battery Installation

Install Battery

 

Trip Indicator Lights

If a new trip unit is being installed, install the trip unit battery.

Install battery holder with battery (A) in trip unit, observing the correct polarity as indicated on the battery compartment.

NOTE: Battery holder with battery is located under the side flap in the cardboard box the trip unit is shipped in.






Press test/reset button (A). All four indicator lights (B) should light. If they do not light, check polarity of battery and retest. If indicator lights still do not light up when test/reset button is pressed, stop installation and contact the local sales office for factory authorized service

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.