48049-137-05EN

Operation Counter

This displays the maximum number of operations (trip or circuit breaker openings) since the circuit breaker was installed. The number is obtained from the circuit breaker communication module (BCM).

Check Operation Counter

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.