48049-137-05EN

Short-Time Protection

Short-Time Protection Switches

MicroLogic 5.0P
Trip Unit

MicroLogic 6.0P
Trip Unit

Short-time protection protects equipment against short circuits.

  • Short-time protection is standard on 5.0P and 6.0P trip units.

  • The short-time pickup (Isd) (A) sets current level (below instantaneous trip level) at which circuit breaker will trip after the preset time delay.

  • The short-time delay (tsd) (B) sets the length of time that the circuit breaker will carry an overcurrent above the short-time pickup current level before tripping.

  • The I2t on/I2t off option provides improved selectivity with downstream protective devices:

    • With I2t off selected, fixed time delay is provided.

    • With I2t on selected, inverse time I2t protection is provided up to 10 x Ir. Above 10 x Ir, fixed time delay is provided.

  • Intermittent currents in the short-time tripping range which do not last sufficiently long to trigger a trip are accumulated and shorten the trip delay appropriately.

  • Short-time protection can be zone-selective interlocked (ZSI) with upstream or downstream circuit breakers. Setting tsd to the 0 setting turns off zone-selective interlocking.

  • Short-time protection uses true RMS measurement.

  • Short-time pickup and delay can be adjusted to provide selectivity with upstream or downstream circuit breakers.

NOTE: Use I2t off with ZSI for proper coordination. Using I2t on with ZSI is not recommended as the delay in the upstream device receiving a restraint signal could result in the trip unit tripping in a time shorter than the published trip curve.

MicroLogic Trip Unit Short-Time Delay Values

Setting Short-Time Delay
I2t off (ms at 10 Ir) (seconds) 0 0.1 0.2 0.3 0.4
I2t on (ms at 10 Ir) (seconds) 0.1 0.2 0.3 0.4
tsd (min. trip) (milliseconds) 20 80 140 230 350
tsd (max. trip) (milliseconds) 80 140 200 320 500
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.