48049-137-05EN

Neutral Protection

Neutral protection protects neutral conductors against overheating.

  • For a three-pole circuit breaker, neutral protection is possible if a neutral current transformer is used.

    • Adjust the neutral using the trip unit keypad.

    • Possible settings are OFF, N/2, N, or 1.6N.

    • Factory setting is OFF.

    • Oversize neutral protection (1.6N) requires use of the appropriate oversize neutral current transformer.

CAUTION
Hazard of equipment damage
If a four-pole circuit breaker neutral pole switch is set to 4P3D setting, the current in the neutral must not exceed the rated current of the circuit breaker. For a three-pole circuit breaker with oversize neutral protection (1.6N), select the appropriate oversize neutral current transformer.
Failure to follow these instructions can result in injury or equipment damage.
  • For a four-pole circuit breaker, set system type using the circuit breaker neutral selector dial .

    • Make fine adjustments using the trip unit keypad, with the circuit breaker dial setting providing the upper limit for adjustment.

    • Factory setting is 4P4D.

  • Neutral protection conductor type has four possible settings:

    • Off—Neutral protection is turned off.

    • N/2—Neutral conductor capacity is one-half that of the line conductors.

    • N—Neutral conductor capacity is the same as that of the line conductors.

    • 1.6N—Neutral conductor capacity is 1.6 times that of the line conductors. (Three-pole circuit breaker only.)

Four-Pole Circuit Breaker Neutral Selector Dial

Neutral Protection Settings for Four-Pole Circuit Breaker

Circuit Breaker Selector Dial Available Keypad Setting
4P 3D Off, N/2, N
3P N/2 N/2
4P 4D N/2,N

MicroLogic Trip Unit Conductor Type

Setting Long-Time Pickup Short-Tme Pickup Instantaneous Ground-Fault Pickup
Trip Unit Neutral Trip Unit Neutral Trip Unit Neutral Trip Unit Neutral
OFF Ir None Isd None Ii None Ig None
N/2 Ir 1/2 Ir Isd 1/2 Isd Ii Ii Ig Ig
N Ir Ir Isd Isd Ii Ii Ig Ig
1.6N Ir 1.6 x Ir Isd 1.6 x Isd* Ii Ii Ig Ig
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.