48049-137-05EN

Trip Unit Operation Verification

Use a test kit connected to the trip unit test plug receptacle (A) to verify trip unit is functioning as desired. See instructions shipped with test kit to perform verification tests.

NOTE: To verify operation of the circuit breaker and trip unit, use primary injection testing. (See Trip Unit Installation Check for more information.)

Verify Trip Unit Operation

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.