48049-137-05EN

Bar Graph Display and Menus

Menus

The MicroLogic P trip unit has a default bar graph display of currents and three different menus which can be accessed using navigation buttons:

A Bar Graph Display—Provides real-time bar graph display of line currents and measurement of line current and neutral current (if applicable) (default display)
B Metering Menu—Provides access to metered values of current, voltage, power, energy and frequency
C Maintenance Menu—Allows user to change the trip unit configuration and provides access to history logs
D Protection Menu—Allows precision adjustments to basic and advanced protection

When the switch cover is closed, the trip unit will return to the bar graph (default) display after 3.5 minutes of no input. (If the switch cover is open, the display stays at the window selected.) To access another menu, press the button that corresponds to the desired menu. The menu appears on the display and the green LED below the menu button lights up.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.