48049-137-05EN

External Power Supply

CAUTION
HAZARD OF Shock, arc flash or Equipment damage
Trip unit and communication module must use separate power supplies.
Failure to follow these instructions can result in injury or equipment damage.

The trip unit can be powered by:

  • 24 Vdc external power supply (recommended).

  • Over 150 V on the bottom circuit breaker terminals on two phases.

  • Over 150 V on the top circuit breaker terminals with external voltage option.

Power Supply Specifications

Function Specification
Power for Trip Unit Alone 24 Vdc, 50 mA
Minimum Input-to-Output Isolation 2400 V
Output (Including Max. 1% Ripple) ±5%
Dielectric Withstand (Input/Output) 3 kV rms
Connections Connections UC3

Power supply is used for:

Graphic screen display when the circuit breaker is open and top fed.

Option of linking an alarm to a relay output.

To maintain date and time when the circuit breaker is open.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.