48049-137-05EN

MicroLogic Setup

MicroLogic Setup

NOTE: If trip unit is connected to a communication network which provides date and time synchronization, date/time cannot be set from trip unit.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.