48049-137-05EN

M2C/M6C Programmable Contacts

M2C/M6C Contacts Setup

  • Available only if M2C/M6C contacts are installed.

  • One alarm per contact.

  • Can select those set up as “alarm” or “trip” under protection menu.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.