48049-137-05EN

Switch Settings

On the face of the trip unit are adjustable switches to allow changing of the LSI or LSIG trip characteristics of the trip unit. Trip units are shipped with the long-time pickup switch set at 1.0 and all other trip unit switches set at their lowest settings. All advanced protection settings are turned “off.”

Fine switch adjustments can be made with the navigation keys. See Switch Settings Adjustment.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.