48049-137-05EN

Zone-Selective Interlocking (ZSI)

The number of devices which can be interlocked are shown in .

ZSI Combinations

Downstream Device (sends output to RIM) Upstream Device (receives input from RIM)
MicroLogic #.0x Trip Units Square D MicroLogic Series B Trip Units Square D
GC-100 Ground-Fault Relay for Equipment Protection
Square D
GC-200 Ground-Fault Relay for Equipment Protection
Merlin Gerin STR58 Trip Units Federal Pioneer USRC and USRCM Trip Units
MicroLogic #.0x Trip Units 15 R R 15 15 R
Square D MicroLogic Series B Trip Units R 26 R R R 15
Square D GC-100 Ground-Fault Relay for Equipment Protection R R 7 R R R
Square D GC-200 Ground-Fault Relay for Equipment Protection 15 R R 15 15 R
Merlin Gerin STR58 Trip Units 15 R R 15 15 R
Merlin Gerin STR53 Trip Units 15 R R 15 15 R
Federal Pioneer USRC and USRCM Trip Units R 15 R R R 15
Square D Add-On Ground Fault Module for Equipment Protection R 5 R R R R

Jumpered Terminals

Wire circuit breakers for zone-selective interlocking.

Circuit breaker terminals are shipped with terminals Z3, Z4 and Z5 jumpered to self-restrain the short-time and ground-fault functions. Remove the jumpers when activating zone-selective interlocking.

NOTE: Use I2t off with ZSI for proper coordination. Using I2t on with ZSI is not recommended as the delay in the upstream device receiving a restraint signal could result in the trip unit tripping in a time shorter than the published trip curve.

ZSI Wiring Example

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.