48049-137-05EN

MicroLogic Setup

Use the Maintenance Menu by pressing the wrench key.

NOTE: If trip unit is connected to a communication network which provides date and time synchronization, date/time cannot be set from trip unit.

See MicroLogic Trip Unit Setup for step-by-step instructions to set up the MicroLogic trip unit.

See Trip Unit Configuration for other trip unit configurations instructions.

MicroLogic Setup

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.