48049-137-05EN

Trip Unit Testing

Trip unit LSIG functions can be tested using primary injection testing or secondary injection testing. Test trip unit using the full-function test kit or hand-held test kit. (See Trip Unit Installation Check for more information.)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.