48049-137-05EN

Graphic Display Navigation Buttons

Graphic Display Screen

Display

The graphic display (A) functions if the trip unit is connected to a 24 Vdc external power supply or there is 150 V on at least two phases. Current alone (from primary injection test set or electrical system) will power the LSIG protection functions, but will not power the display.

Navigation buttons (B):

Metering Menu Button—Provides access to metering menus

Maintenance Menu Button—Provides access to maintenance menus

Protection Menu Button—Provides access to protection menus

Down Button—Moves cursor downward or decreases setting value

Up Button—Moves cursor upward or increases setting value

Enter Button—Selects an option from a list or enters the set values

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.