48049-137-05EN

M2C/M6C Programmable Contacts

If M2C or M6C contact kit is installed, use “Contacts M2C/M6C” menu to set alarm type and operational mode. The M2C kit has S1 and S2 contacts. The M6C kit has S1, S2, S3, S4, S5 and S6 contacts.

M2C/M6C Contact Kits Setup

   

Set M2C/M6C Contact Alarm Type

1. Enter M2C/M6C contacts alarm type into trip unit memory. Available alarms are:

Ir Long-time pickup
Ii Instantaneous pickup
Isd Short-time pickup
Ground-fault current
Ground-fault alarm
Iunbal Current unbalanced
Iamax Phase A demand overcurrent
Ibmax Phase B demand overcurrent
Icmax Phase C demand overcurrent
Inmax Neutral demand overcurrent
Vmin Voltage is below set minimum
Vmax Voltage is above set maximum
Vunbal Voltage unbalanced
rPmax Reversed power
Fmin Frequency is below set minimum
Fmax Frequency is above set maximum
ΦF rot Phase rotation
Ished Current shedding
Pshed Power shedding
Not Selected No alarms selected

2. Set up M2C/M6C contact alarm mode. Contact modes available are:
  • Latching contact—Stays latched until reset

  • Nonlatching contact—Drops out after fault is removed.

  • Time Delay—Delay placed on contacts

For troubleshooting purposes only the following modes are available:

  • Locked 0—Contacts are locked open

  • Locked 1—Contacts are locked closed

For short-time, instantaneous and ground fault (SIG) alarms only:

  • Each alarm occurrence will activate the relay and will signal and continue to signal an alarm until the trip unit test/reset button is pressed.

  • This “latching behavior occurs regardless of whether “latching” or “nonlatching” contact mode was used during alarm setup.

Set M2C/M6C Contact Alarm Mode

3.

Reset displays states of relays and allows them to be reset.

NOTE: Select reset option under the M2C/M6C menu to reset all alarms. The test/reset button on the trip unit will reset the trip unit so that it will stop activating the alarm, but does not reset the M2C/M6C contact.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.